New release of Allied Vision’s VIMBA X SDK, now supporting SVS-Vistek cameras

Product News

Allied Vision releases new version of its Software Development Kit VIMBA X

Allied Vision has released a new version of the comprehensive and fully GenICam-compliant Software Development Kit Vimba X. Besides new attractive features for image acquisition and camera control such as the Multi-ROI Widget and TCP support for Linux x64, the new Vimba X SDK offers another step towards integrated TKH Vision solutions. The new release not only supports Allied Vision’s machine vision and embedded vision cameras. Now, also high-resolution and high-bandwidth GigE Vision, USB3 Vision, and CoaXPress cameras from the TKH Vision sister company SVS-Vistek GmbH are officially supported and enabled by default.

This extension allows customers to use cameras from both companies with the same SDK within the same application. Mixed configurations in different applications are also possible, which considerably expands the range of options for customers. Being able to use the same SDK for different cameras significantly reduces development time and costs.

At the same time, SVS-Vistek is releasing a new version of the SDK SVCam now supporting the main functionality of Allied Vision’s Alvium cameras with GigE Vision and USB3 Vision interface.

New Multi-ROI Widget in Vimba X Viewer
The new widget makes using and defining multiple Region-of-Interests (ROI) much easier and more comfortable. It is now very user-friendly to see which ROIs are activated, and what size they are and where they are positioned. For a precise positioning of the ROI, previously saved images can be loaded and used.  Additionally, the user can define different values for specific image features for each single ROI (e.g. different contrast, hue, or saturation values), a feature unique to Allied Vision’s Alvium cameras.

Further improvements and new features include:

  • Completely revamped Event Viewer for easier access and higher user-friendliness
  • Updated Python API (VmbPy) with improved auto-completion. 

Vimba X 2024-1 is available for the following operating systems:

  • Windows: Windows 10 21H2 LTSC, Windows 11 23H2
  • Linux: Ubuntu 24.04 LTS, Debian 12.6
  • ARM: JetpackTM 5.1.0, AGX OrinTM DevKit (all TLs)