Vimba Defective Pixel Manager - Release Notes Version: 1.1.3 Date: June 2021 ============================================= Prerequisites ------------- - Vimba 5.0 for Windows or higher (install at least the transport layers for your camera interface and the Vimba driver for Allied Vision USB cameras). You can use Vimba Defective Pixel Manager on the same drive or on a different drive than Vimba. - Allied Vision GigE or USB camera with defect masking or defect pixel correction feature Supported cameras ----------------- Alvium USB 1800 U (U-1620, 2040, 2460, 2050, 040m) Mako G Mako G-030, Mako G-131, Mako G-192, Mako G-503 Manta Manta G-223, Manta G-419, Manta G-1620, Manta G-2040, Manta G-2460 Prosilica GT GT4400, GT5400, GT6400, GT5120, GT5120NIR, GT4090, GT4096 Unsupported cameras ------------------- - Goldeye-G - Mako G-223, Mako G-419 - Prosilica GT2050, GT2000 Support of discontinued cameras ------------------------------- Discontinued cameras were not tested with the latest version Vimba Defective Pixel Manager. However, correcting defective pixels should be possible with: - Mako U - Prosilica GT4905, GT4907, GT6600 Known issues ------------ - Alvium: - If error -11 occurs, reset the camera by software command or unplug it for a short time. This is a camera firmware issue. - To apply a correction set by default, open the camera in Vimba Viewer, go to CorrectionControl, and select the desired correction set as Default. - Manta-G and Mako-G: - Only 100 defective pixels can be loaded into these cameras. - Prosilica GT 4-tap cameras: - Column Defect: Height cannot be entered - Prosilica GT4905, GT4907, and GT6600: - These cameras cannot delete all defects (zero-size memory writes are not accepted) - Pixel row defects: Editing the width pixel value is not possible - Depending on camera resolution and zoom factor, some pixel defects appear shifted in the image. Workaround: Select a different zoom factor. This is a qt issue. - High values of auto exposure may cause image freeze. - Changing BlackLevel values significantly may cause image freeze.