Vimba X Defective Pixel Manager - Release Notes Version: 2.0.0 Date: April 2023 ============================================= Prerequisites ------------- Please install Vimba X (Windows, Linux, or ARM). Supported cameras ----------------- Alvium cameras with DPC feature (all GigE and USB models, all CSI-2 models with GenICam support). Manta Manta G-223, Manta G-419, Manta G-1620, Manta G-2040, Manta G-2460 Mako G Mako G-030, Mako G-131, Mako G-192, Mako G-503 Known issues ------------ - Sometimes, cameras are listed twice. Workaround: refresh the camera list. - If a camera is plugged in while the application is already open, it may be listed as "DPC unsupported". Workaround: Refresh the camera list. - If you have installed multiple GigE or USB transport layers, startup may take a long time and each camera is listed multiple times. Workaround: Remove VmbC.xml and replace it with VmbC.xml of Vimba X. - Blacklevel is not changed during acquisition (Alvium cameras). Workaround: Stop image acquisition to change the value. - Importing or uploading a file with many pixel defects may take several minutes. Please wait until the process is complete. Changes compared to Vimba Defective Pixel Manager ------------------------------------------------- - Added Alvium 5GigE support, removed Prosilica GT support - Added Linux and ARM compatibility - Several bug fixes