カメラセレクター(選択ツール)
ブックマーク

Now Available: Alvium Camera Kit for NVIDIA Jetson Nano Developer Kit

ニュースリスト

NewsProduct News

Allied Vision releases first Alvium CSI-2 Camera Kit for easy integration

To make the integration of Alvium CSI-2 cameras into any system as easy as possible Allied Vision will be releasing various Alvium Camera Kits consisting of an Alvium CSI-2 camera, a set of accessories and a ready to use SD card image. The first kit available is the Alvium Camera Kit tailored for the NVIDIA Jetson Nano Developer Kit.


Alvium Camera Kit for NVIDIA Jetson Nano Developer Kit

The new Alvium Camera Kit for NVIDIA Jetson Nano Developer Kit consists of:

  • 5 Megapixel CSI-2 camera Alvium 1500 C-500c color, with S-Mount and open housing, equipped with ON Semi’s AR0521 CMOS sensor
  • Allied Vision lens (8mm focal length)
  • CSI-2 adapter board for the NVIDIA Jetson Nano Developer Kit
  • 2 CSI-2 cables
  • Tripod mounting plate
  • Pre-configured SD card image with included CSI-2 Driver available online

The complete package is available at an attractive price of 199€ or $229. The excellent price-performance ratio and the complete set of required accessories offer system developers to jump start in the prototyping phase and gives a unique opportunity to embed the Alvium camera into a system or project.

"Partnering with a visual computing innovation leader like NVIDIA strengthens our vision to help people to reach their imaging goals. We look forward to supporting developers with industrial grade camera technology and image capture solutions for their industrial inspection, medical and scientific imaging, traffic monitoring and other emerging applications", said Mark Schenk, Product Manager at Allied Vision.

"The Alvium industrial CSI-2 camera kit for the Jetson Nano offers developers an easy to use platform for vision-based embedded applications. Allied Vision’s support of the NVIDIA Jetson platform brings valuable experience in industrial cameras into our partner ecosystem", added Murali Gopalakrishna, Head of Product Management for Autonomous Machines at NVIDIA.


CSI-2 driver for NVIDIA Jetson System-on-Modules

Together with this Alvium Camera Kit Allied Vision provides one common CSI-2 driver for NVIDIA's Jetson systems that is compatible with all Jetson family System-on-Modules (Jetson Nano, Jetson TX2 and Jetson AGX Xavier) and the NVIDIA JetPack SDK, regardless of the choice of Alvium camera used. For long-term availability Allied Vision published the CSI-2 driver on Github.com and plans to further maintain and support future versions of the JetPack SDK, to guarantee easy integration without the need for another Driver.

Allied Vision is an NVIDIA Preferred Partner and Jetson Partner. The NVIDIA Jetson family of products provides the performance and power efficiency to run autonomous machines faster and with less power in a compact form factor, bringing the power of modern AI, deep learning, and inference to embedded systems at the edge.

ニュースリスト