相机选型工具
在线咨询
点击或扫码咨询
(无需添加好友)

基于索尼CCD传感器相机的末次购买和末次发货期限

采用索尼 CCD 传感器项目的抉择困难:即刻转型还是持续坚守?

我们支持您针对自身项目寻找更好的应对方案。

了解更多

Kudan和Allied Vision

Kudan与Allied Vision的合作备受期待。Kudan Grand SLAM软件现已支持Nerian Ruby 3D深度相机,并随同Kudan自主移动机器人的移动机器人开发套件提供。

 

了解更多

高分辨率短波红外相机

即将发布:

搭载Sony IMX992/993传感器的Alvium短波红外相机

 

了解更多

Goldeye XSWIR LP 扩展型短波红外相机

Goldeye XSWIR 扩展型短波红外相机
像素尺寸低至 2.2 µm,集成 TEC2 双重冷却技术


了解更多

 

为您的应用选择合适的相机

 

前往相机选型工具

 

专注于您的需求

我们不止于开发相机,我们探求答案。

在Allied Vision,我们致力通过计算机视觉数码相机助力客户达成目标。这项技术为各行各业的企业机构开辟了一系列全新机遇。我们的相机产品最初基于制造商需求打造,现已扩展到各个领域,包括科学与研究、医学成像、交通监控和运动分析。

 

鉴于我们的客户面临着各种应用挑战,我们始终致力提供灵活多样的相机产品线。这也是我们采用模块化相机设计的原因所在。最终,我们提供了各式传感器、镜头接口、滤镜、主板型号选择以及更多其他选项,最大限度提高灵活性。

 

了解更多

“相”您所想

可精准满足您需求的相机技术

我们的工程师设计的数码相机提供了海量的分辨率、帧率、带宽、接口、光谱灵敏度、传感器技术和技术平台选项。我们为此打造了模块化概念,确保相机可灵活适应您的应用需求,而不对您的应用设限。

 

熟谙如何针对不同应用场景寻找最适宜的相机解决方案。这既包括了数码相机本身,也兼顾了适配的镜头连接硬件以及软件接口。我们的工作是在任何场合以直观的方式可靠地输出所需的图像。

 

 

了解我们的产品

从嵌入式应用到科研

面向您应用的视觉解决方案

应您所需

技术支持

在图像处理项目的全生命周期中,Allied Vision为您提供全程支持。我们可随时助您将相机集成至自有系统,解决软件相关问题,确保系统在购入相机的数年内仍能发挥一贯性能。

 

我们的专家将为数字相机及其外设,以及它们与您机器视觉系统的整合提供专业的建议、设计、制造和支持。

查看技术文档和下载

时刻关注最新信息!

最新资讯

Preview: Alvium cameras supporting Optotune’s liquid lenses at Automate

Company News

Allied Vision will showcase an Alvium camera with a liquid lens from Optotune in Chicago from May 6 - 9, 2024

Allied Vision, a world leader in camera technology and image capture solutions, and Optotune AG, a market leader in liquid lenses, will present an integrated system at Automate, booth #5255.  Allied Vision’s compact and flexible Alvium cameras now support Optotune liquid lenses enabling customers in a variety of markets and applications such as industrial inspection, facial recognition, barcode reading, drones, mail/package sorting, robotics, and medical and scientific imaging.


Live Demo
At Automate, on display will be the Alvium 1800 U-507c with Sony IMX264 which runs 34.0 frames per second at 5.1 MP resolution. The lens from Optotune is the ELM-25-2.8-18-C with the ECC-1C controller. The camera will be looking at multiple other Allied Vision cameras set up all at different distances and interchanging the focus between each one. Allied Vision's VimbaX SDK combined with custom firmware, officially available in Q3 this year, allows the camera to control the lens using the GenICam standard. The concept is to show the ability to rapidly change working distances; giving customers the flexibility in applications where objects are moving quickly or where the distance between the camera and the object changes frequently.


Benefits of Liquid Lens Technology
Optotune has co-designed with its optics partners a series of lens modules developed around its electrically tunable lenses resulting in optically optimized and integrated solutions that simplify the design of vision systems. Customers benefit from fully tested modules, low f-numbers without vignetting and compact solutions. Liquid lenses have no moving parts making them durable and reliable—they also offer flexibility and versatility because they can be remotely adjusted and integrated for various applications at once. Allied Vision looks forward to continuing to support its customers with this technology from Optotune.

 

Allied Vision at Automate:

  • TKH Vision Booth #5255
  • May 6 - 9, 2024 
  • McCornick Place, Chicago, Illinois, USA